Create a New ViewX Client - System Connection

You can use the ClearSCADA Client Applet to create a new ViewX client - system connection. You need to create a client - system connection for each outgoing ViewX client connection i.e. every connection that the client uses to send signals to the system server(s).

When you have created a new connection, you will need to configure it so that the client can use it to communicate with the system server(s).

To create a new ViewX client - server connection use the topics in the order they are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Alternatively, you can create a connection by creating or editing a Systems.xml file manually Use the Systems.xml File to Set Up a ViewX Client Connection.


Disclaimer

ClearSCADA 2017 R3