Edit an Existing ViewX Client - Third Party OPC Server Connection

You can use the ClearSCADA Client Applet to change the configuration of an existing ViewX client - Third Party OPC server connection. This is useful when you need to alter the way the client - OPC server connection works, for example, you may need to rectify a mistake such as having selected the wrong Type of OPC server.

To edit an existing ViewX client - Third Party OPC server connection:

  1. On the ViewX client, use the Windows Start menu to access ClearSCADA’s Configure Connections option and run the ClearSCADA Client applet.
  2. Select the ViewX - Third Party OPC server connection that you want to edit.
  3. Select the Edit button to display the ClearSCADA Client Configuration window.
  4. Use the ClearSCADA Client Configuration window to change the System Name, Type, Visible in ViewX and Node settings as required. For more information on these settings, Create a Connection between a ViewX Client and a Third Party OPC Server.

Disclaimer

ClearSCADA 2017 R3