Failed Third Party ODBC Client - System Connections

If the Third Party ODBC client - system connection cannot be established, the ODBC client will be unable to connect to ClearSCADA.

The connection may fail to establish if:

The Third Party ODBC Client - system connection works in the same way as a ViewX - system except that it uses a different license and it requires Data Access components (to be installed on the computer that is running the Third Party ODBC applications). The firewall rules for Third Party ODBC Client - System connections are the same as those for ViewX - system connections.

Further Information

Firewall Settings for Client - System and Server Advise Connections.


Disclaimer

ClearSCADA 2017 R3