Working with Single and Multiple Databases

A ViewX client can be configured to access a single ClearSCADA database or multiple ClearSCADA databases. Each ClearSCADA database is independent and runs as a ClearSCADA system on a ClearSCADA server (or on multiple ClearSCADA servers if used in a multi-server redundant architecture). This means you can use a single ViewX client to:

For more information on single and multi-database setups, please refer to the following sections:

A ViewX client can connect to a maximum of 64 databases.


Disclaimer

ClearSCADA 2017 R3