OPC Time Format

You should enter periods of time in the OPC Time Format, which consists of a time value and a time unit. For instance, 10S is the OPC time format for ten seconds.

You use the OPC time format, for instance, to specify the maximum call length for a PSTN outstation.


If you are required to specify a time period, either:

or:


Disclaimer

ClearSCADA 2017 R3