Printing

ClearSCADA provides you with the facility to print a variety of data output. You can configure printing to be done manually or to occur automatically. The following is a list of features with which you can use the print facility:

There are two printing options available for various features within ClearSCADA:

In Microsoft® Windows®, you can only access those printers that are associated with your Windows user accounts. The ClearSCADA server runs as a service, so a system administrator needs to specify a Windows user account in the ClearSCADA server configuration to allow the ClearSCADA server to access the required printers, see Printer Settings.


Disclaimer

ClearSCADA 2017 R3