Resolving Errors Detected While Attempting to Save Configuration

Should a conflict or problem be detected when an attempt is made to save configuration changes, a red cross will overlay the icon on the document window tab or title bar.

Should this occur, the document window will enter diagnostic mode. ClearSCADA will overlay the document window with a diagnostic message that provides you with a choice of options. The options vary depending on the reason for the document entering diagnostic mode. Examples of diagnostic mode messages and options are given below.

Configuration Conflicts

A configuration conflict might occur if a user attempts to save configuration changes to a database item for which another user has made separate configuration changes in the meantime. The buttons that the resulting diagnostic message provides vary, depending on the detected conflict and its context.

For example, with the display shown above, three buttons are offered:

Problem Detected when Attempting to Save Configuration

If ClearSCADA detects a problem when an attempt is made to save configuration changes, the diagnostic message will summarize the detected problem. The buttons that the diagnostic message provides vary, depending on the detected conflict and its context.

For example, with the display shown above, two buttons are offered:

Further Information

Checking for Invalid Configuration.


Disclaimer

ClearSCADA 2017 R3