Yearly Schedule

The display for a Yearly Schedule looks similar to a Monthly Schedule, with the addition of a tab for each month of the year.

You can define processes to start from any 5-minute interval (for instance, 12:00, 12:05, 12:10, or 12:15) on any day of any month in the year.

You need to configure a separate Yearly Schedule for any action(s) that require triggering at different times or on different months to other scheduled action(s). For instance, if some actions need triggering during March, June, and September, and another set of actions need triggering during January, March, and July, you will need to configure two Yearly Schedules, one for each set of actions.

When you are editing the Schedule Display, the time indicated by the position of the cursor is displayed in the format D, HH:MM (where D = date, HH = hours, MM = minutes). For example, 4, 05:35 indicates 5:35am on the 4th day of the month that is on display.

You may find it easier to maximize the Schedule Display while adding processes, so that you can readily select the required times.

Further Information

Set up a Schedule.


Disclaimer

ClearSCADA 2017 R3