Update an Output Point's Value Immediately Following a Successful Control Action

This section applies to analog and digital output points.

On some drivers you can specify whether ClearSCADA is to update an output point's value immediately following a successful control action, or whether it is only to update the point's value after the next poll. With output points that support this feature, you use the Update Point on Successful Action check box on the point's Control tab to specify the requirements.

Either:

Or:


Disclaimer

ClearSCADA 2017 R3