Define the Page Margins

In addition to using the Printing section of the Crystal Report tab to Define the Print Properties, you need to use the fields within the Margins section of the tab to define the page margins for reports that are printed using the Print Report pick action.

Enter the margin sizes in millimeters. If you are specifying small margins, you should consider the capabilities of your system printer(s), as they may only support margins of a certain size.

(If you print a report directly from the Crystal Reports application, you need to specify the page setup from within the Crystal Reports application, rather than on this Form. If you use the Crystal Reports Viewer to display a previously generated report in ViewX, and then choose to print that report, you can specify the print settings using the Print option, available from the ViewX File menu. You then use ViewX’s Print menu option to print the report. (For more information on the latter, see Using the Crystal Reports Viewer.))


Disclaimer

ClearSCADA 2017 R3