Export the Report to a File on a Disk

You can export a report to disk automatically. You can use this feature to provide long-term offline storage of reports on a variety of devices, including removable hard disks, CD-Rs, CD-RWs, DVD-Rs, and DVD-RAM, depending on your system hardware.

If you are using this feature to store reports on removable media, the media has to be at the required location and available for use. For example, if the report is to be stored on a CD-R, you need to check that a CD-R is in the CD-RW drive of the server before a report is due to be exported.

To allow ClearSCADA to export a report to a file on a disk, you need to specify the File on Disk Destination on the Export Destination tab, and then use the tab to specify these properties:


Disclaimer

ClearSCADA 2017 R3