Generate Report

Associated with: Crystal Reports.

Security permission required to access this pick action: Control.

ATTENTION:Generation of large or complex reports, or reports that query historic table(s), can have a temporary adverse effect on the system. We advise that such reports are generated when little communications traffic is expected on a ClearSCADA system—for example in the early hours of the morning.

Be aware that if a report is configured to enable it to be displayed on an Original WebX client in addition to a ViewX client or WebX client, ClearSCADA will generate two versions of that report whenever the Generate Report pick action is used.

Use the Generate Report pick action to generate a report. When generated, a report is either:

If a report uses Parameters (see Parameter Field), a window is displayed whenever the Generate Report pick action is selected. The window allows you to restrict the data that is included in the generated report. The prompts and options that appear in such a window are specified by the engineer that configured the report parameters—see your system administrator for further information.

Example:

If using this pick action with the Automation Interface, you need to specify the method name Generate.

Should you experience difficulties when generating reports, see The Server Fails to Generate a Report.


Disclaimer

ClearSCADA 2017 R3