Specify a Trip Sequence for a Time

To specify a trip sequence for a time, you enter the trip code:

%T<format>%

where <format> is one or more of the Windows® picture string time formats that ClearSCADA supports (see Supported Trip Codes for Times).

To specify the time that ClearSCADA substitutes for the trip code, you use the Trip Sequence Time field on the appropriate tab of the Crystal Report Form.

The default of NOW results in a time of ‘now’ exactly. If an offset time stamp is required, you can specify another time value in the OPC Relative Time Format.

For examples of how to use the Trip Sequence Time in conjunction with the trip sequences that you specify for your exported reports, see Specify the Trip Sequence Time.

Further Information

Resolving any Trip Sequence Errors.


Disclaimer

ClearSCADA 2017 R3