ViewX Client Component

You need to install the ViewX Client Crystal Reports component on the ViewX clients in your system.

The Crystal Reports component is only displayed in the Installation Wizard on machines on which the Crystal Reports 32-bit runtime components are installed (see Install Crystal Reports).

You also need to install other software. For the step-by-step procedure that you should follow in order to install the required software on your system’s server(s) and ViewX clients, see Install Crystal Reports.


Disclaimer

ClearSCADA 2017 R3