Working with the Reports List

The Reports List is Crystal Reports specific—it is only available on systems that have the Crystal Reports driver installed. You use the Reports List to display a list of the Reports on your system. You can display the List from the Queries Bar or the web interface, as you would any other Lists (see the ClearSCADA Guide to Lists).

As with other Lists, the Reports List consists of rows and columns. Each row represents an individual report entry, and each column contains information about a specific value for that report.

The Reports List contains these column headings:

As with other Lists, you can right-click on an entry in the List to display a context sensitive menu. From this menu, you can select options to display further information about a Report, or request various actions. For information on the actions that are Crystal Reports specific, see Using Actions Associated with Crystal Reports.

ClearSCADA displays the entries on the List using a series of system colors. For information on the driver-specific colors associated with the Crystal Reports List, see Crystal Reports Specific Colors.


Disclaimer

ClearSCADA 2017 R3