Alarm Conditions Section

In the Database Schema, the Alarm Conditions section shows information about the Alarm Conditions of the class.

Example:

The Alarm Conditions section for the CPointAlg class shows information about the alarm conditions that are available to analog points.

For each Alarm Condition of the class, the following information is shown:

As the Alarm Conditions are of the CAlarm class, they also provide access to the Fields and Methods for the CAlarm class.


Disclaimer

ClearSCADA 2017 R3