Display Information about All Classes

You can use the ClearSCADA Database Schema to display information about every class, not just those classes that are creatable. By displaying the All Classes 'page', you can:

To display information about all classes:

  1. Access the Database Schema.
  2. Select the List All Classes hyperlink.
    The All Classes 'page' is displayed.

You can select a hyperlink for each class of item. This displays information about the relevant class.

Further Information

Createable classes and non-createable classes: see Classes.


Disclaimer

ClearSCADA 2017 R3