Abort Pulse

Associated with: Pulse actions

Security permission required to access this pick action: Control

This pick action is only available on a pulse action if an Inching or Control action is currently active or awaiting execution on a pulse action (as indicates by the pulse action’s Control Active status attribute, and the Point Action system color).

Use the Abort Pulse pick action to abort the currently active pulse control.

If using this pick action with the Automation Interface, you need to specify the method name Abort.


Disclaimer

ClearSCADA 2017 R3