Last Outgoing Call Lost Comms

Associated with: PSTN outstations or outstations on which PSTN fallback is enabled

This attribute displays the date and time of the last outgoing call for which communications were established, but which then terminated unexpectedly. The attribute is only displayed once such a call has occurred.

Example:

20/Mar/2008 16:48:05.971

Also see the Outgoing Calls attribute, which provides a summary of the outgoing calls since the statistics were last reset.


Disclaimer

ClearSCADA 2017 R3