Logged Time

Associated with: Points that have logged data

This status attribute indicates the date and time of the latest logged (time stamped) data to be retrieved for a point.

If logged data is retrieved for the point, this attribute is updated whenever new logged data is retrieved, regardless of whether ClearSCADA actually stores that data historically. (The time indicates the time stamp that was reported with the data, not the time that ClearSCADA stores any such data historically.)

Use this status attribute in conjunction with other Logged attributes (such as Logged State and Logged Value).


Disclaimer

ClearSCADA 2017 R3