Point Statistics

Associated with: Scanners; outstations; Slave outstations

This status attribute displays statistics about an outstation’s or scanner’s point data. The attribute lists the number of point updates, historic records, point alarms and events that ClearSCADA has retrieved from the outstation or scanner since the statistics were last reset.

Example:

24 updates, 26 historic, 0 alarms, 3 events since 11/Nov/2007 11:57:49.111

Also see Comms Statistics.

Further Information

Reset Point Statistics.


Disclaimer

ClearSCADA 2017 R3