Put Aside Quality

Associated with: Points for which a local Override is currently in force

This status attribute indicates the reliability of the point data that was ‘put aside’ at the time that the current local Override came into force.

For a comprehensive list of quality values, see Quality.

Use the status attribute in conjunction with the other Put Aside status attributes (such as Put Aside State and Put Aside Value) to ascertain further information about the point data that was ‘put aside’.


Disclaimer

ClearSCADA 2017 R3