Queue Check Box

A Queue check box may be displayed on some pick action windows:


The Queue check box is only displayed:

With a pick action window in which the Queue check box is displayed:

If ClearSCADA is communicating with the outstation at the time that the pick action is triggered, ClearSCADA will immediately send the request to the outstation, regardless of the Queue check box’s setting.

(Be aware that any queued requests for an item will be deleted automatically should the item’s configuration become invalid.)

Further Information

Optionally Queue Pick Action Requests on PSTN and ‘On Demand’Outstations.


Disclaimer

ClearSCADA 2017 R3