Refresh

Associated with: Scanners; outstations that support this feature

Security permission required to access this pick action: Retrieve Data

ClearSCADA typically scans devices for data on a scheduled basis. If required, you can use the Refresh pick action to scan a device on demand. Select the Refresh pick action to request a current data update of the points on a particular outstation or scanner. Depending on the protocol, a Refresh either:

The Refresh pick action is only available on an outstation that communicates via PSTN while that outstation is on line (for instance, during an Open Line call). When a call is not in progress, use the One Shot pick action to contact the outstation and ‘refresh’ that outstation’s data.

Do not confuse this Refresh pick action with the Refresh menu options or buttons that are available for various ClearSCADA displays, such as:


Disclaimer

ClearSCADA 2017 R3