SIN

The SIN function is a mathematical function that returns the Sine (radians) of a number. The SIN function returns a real value.

Function Name

SIN

Description

Returns the Sine (radians) of a number

Arguments

SIN(INTEGER or REAL)

Where:

  • INTEGER or REAL and is the numerical expression upon which the SIN function is to be used.

For more information on integers and real values, see Number (Integer or Real).

Returns

REAL

The Sine (Radians) of the input number.

Example:

SIN(PI() /2)

The output is 1.


Disclaimer

ClearSCADA 2017 R3