SQRT

The SQRT function is a mathematical function that returns the square root of a number as a real value.

Function Name

SQRT

Description

Returns the square root of a number

Arguments

SQRT(INTEGER or REAL)

Where:

  • INTEGER or REAL and is the numerical expression upon which the SQRT function is to be used.

For more information on integers and real values, see Number (Integer or Real).

Returns

REAL

The square root of the input number.

Example:

SQRT(4)

The output is 2


Disclaimer

ClearSCADA 2017 R3