String

A string value is one or more Unicode characters (letters, numbers, and punctuation characters). You can include a string in your expressions by enclosing the string characters in single quotation marks, for example:

'This is a string value.'


The string above is returned as:

This is a string value.


If you need to include single quotation marks as part of the string, simply enter 2 single quotations. For example:

'Don''t'


The string above is returned as:

Don't


To indicate a string, use single quotation marks ' '. Do not use double quotation marks “ “ as these are for indicating tags.


Disclaimer

ClearSCADA 2017 R3