Filter Wildcards

When the Is Like or Is Not Like Filter Condition Types are used to filter a List such as an Events List, Alarm Summary, Queries List, or Historic List, you can include wildcard characters in the filter criteria. Wildcard characters allow a single filter value to match multiple ClearSCADA database values. There are two wildcard characters:

To include a wildcard character in a search without causing the wildcard to match other characters, enter a backslash (\) before the wildcard character. For example PUMP\_1 will only match PUMP_1, and will not match PUMP11, or PUMPA1.

Further Information

The filter wildcards that are supported by Alarms Lists and Alarm Banner differ to the above—for information, see Filter Wildcards in the ClearSCADA Guide to Alarms.


Disclaimer

ClearSCADA 2017 R3