Add Variables to a Function Block Diagram

Each value that is read or written by your Function Block Diagram is represented by a variable or a constant. Constant values are values that are fixed and are described in Add a Constant Value to a Function Block Diagram. Variable values change according to the data that is stored in your system and the calculations that are performed on it.

There are 2 types of variable:

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3