Animating an Object to Execute a Script

The Pick Action Configuration Wizard allows you to create three types of script animations:

However, you can also create these script animations manually, by creating animations for the PickType and PickParam properties.


For a Call Specific Function animation, you need to configure the animations as:

For an Execute Code Fragment animation, you need to configure the animations as:

For an Execute Code Fragment on Top Level Mimic animation, you need to configure the animations as:


Disclaimer

ClearSCADA 2017 R3