Displaying the Animations Window

To access the animation properties for an object, you need to display its Animations window. The Animations window contains a list of the animation properties that are available for the selected Mimic object and shows any expressions that are in place.

To display the Animations window:

  1. Display the Mimic object's Properties window by double-clicking on the Mimic object (with the Mimic in Design mode).
  2. Select the General tab.
  3. Select the Animations button.

Alternatively, right-click on the Mimic object and select the Animations option from the context sensitive menu.

For information on the Animations window settings, see Using the Animations Window.


Disclaimer

ClearSCADA 2017 R3