Editing an Embedded Alarms List

When you have added an embedded Alarms List to a Mimic, you can access its Embedded Alarms List Properties window to edit its settings. To display the window, double-click on the object on the Mimic. (For other ways of displaying the window, see Display the Properties Window for an Object on a Mimic.)

The Embedded Alarms List Properties window has three tabs: General, List Font, and Header Font. These tabs work in the same way as the General, List Font, and Header Font tabs on the Embedded List Properties window, except that they apply to the various parts of the Alarms list (see Editing an Embedded Query List).

However, there are some exceptions:


Disclaimer

ClearSCADA 2017 R3