Enable and Disable a Custom Pick Action Menu

You can use the Pick Menu window to enable and disable a custom pick action menu. Typically, you would not use the Disabled check box on the Pick Menu window as you would use an animation to control whether the pick action menu is available. However, you can make a custom pick action menu inaccessible if required:

To enable or disable a custom pick action menu:

  1. Display the Pick Menu window (see Using the Pick Menu Window).
  2. Either:
    • Select the Disabled check box to make the custom pick action menu unavailable.
    • Clear the Disabled check box to enable the pick action menu so that users can access its options.
  3. Select the OK button to confirm.

Disclaimer

ClearSCADA 2017 R3