FlashFillAlpha

The FlashFillAlpha property defines the amount of transparency that is applied to the FlashFillColour. This works in exactly the same way as the FillAlpha property, except that it applies to the alternate color that is used in the flash effect.


Disclaimer

ClearSCADA 2017 R3