Remove a Custom Pick Action or Custom Pick Action Menu

You can remove a custom pick action or custom pick action menu as required:

  1. Display the Pick Menu window (see Using the Pick Menu Window).
  2. Select the pick action or pick action menu that you want to remove, then select the Remove button.
    The action or action menu is removed.

Disclaimer

ClearSCADA 2017 R3