Test Custom Pick Action Menus

When you are creating custom menus, you can use the Test button on the Pick Menu window to see how the pick action menu will appear when selected on a Mimic. When you select the Test button, the custom pick action menu is displayed.

The Test feature is only designed to show a preview of your custom menu—the options on the custom menu will not have any affect on the system.

To test a custom pick action menu:

  1. Display the Pick Menu window (see Using the Pick Menu Window).
  2. Create the custom pick action menu by adding pick action menus, pick actions, and separator lines as required.
  3. Select the Test button.
    The pick action menu is displayed. It shows the various branches that you have created as part of the menu's hierarchy.


Disclaimer

ClearSCADA 2017 R3