Access Your Operator Document Stores on a WebX Client
            ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of ClearSCADA. For information about the WebX client that is supported by ClearSCADA 2015 R1 onwards, for which the web server is hosted using IIS, click here.
Your user account can be associated with up to six Operator Document Stores.
To access your Operator Document Stores from a WebX client:
- Log on to WebX (see Log On to a WebX Client).
 - Select the Documents button 
    
on the navigation bar.
The top level of your Operator Document Stores is displayed.

 - Navigate the hierarchy as you would the ClearSCADA database, to locate the document you require (see  Use the WebX Interface).
        
        
For example:
- Select a hyperlink in the Children section to access an operator document, or another level of your Operator Document Stores hierarchy.
        
        
or:
 - Select the hyperlink in the Parent section to display the group that contains the item or page you are currently viewing.
 

 - Select a hyperlink in the Children section to access an operator document, or another level of your Operator Document Stores hierarchy.
        
        
 - Select the hyperlink that indicates the required document’s name.
The selected Operator Document is displayed.