Configure the Performance Monitor Properties

Use the fields on the Performance Monitor tab to define the driver-specific properties of an analog point. For information on those fields that are common to points on many simple drivers, see Configure Common Point Properties in the ClearSCADA Guide to Simple Drivers. Fields that are specific to analog points on the Performance Monitor driver are described below.


Disclaimer

ClearSCADA 2017 R3