Expressions.expr-primary-datetime
            A date, time or timestamp value
Format
{ DATE | TIME | TIMESTAMP } { 'Interval' | ? | ( IntervalExpr ) }
Remarks
Specifies a date, time or timestamp value.
The DATE, TIME, or TIMSTAMP keyword is followed by the DateTime value.
The DateTime value can be one of the following:
- A string literal defining the interval value.
 - A parameter marker.
 - A string expression enclosed in parentheses.
 
The resulting string is interpreted as an SQL date, time or timestamp literal. The following table describes the required format for each type:
| Type | Format | 
|---|---|
| DATE | YYYY-MM-DD | 
| TIME | HH:MM:SS[.FFFFFF] | 
| TIMESTAMP | YYYY-MM-DD HH:MM:SS[.FFFFFF] | 
For TIME and TIMESTAMP types, the fractional seconds part [.FFFFFF] is optional
DATE '2007-01-31'
TIME '12:55:00.000'
TIMESTAMP ('2007-01-31' || ?)
	DATE ?