Expressions.expr-primary-odbc-function
            An ODBC function
Format
expr-primary-odbc-timestampadd |
expr-primary-odbc-timestampdiff
Remarks
An ODBC function can be any of the following:
- A TIMESTAMPADD function. Refer to expr-primary-odbc-timestampadd for more details.
 - A TIMESTAMPDIFF function. Refer to expr-primary-odbc-timestampdiff for more details.
 
{ FN TIMESTAMPADD( SQL_TSI_SECOND, 15, TIMESTAMP '2006-08-02 00:00:00' ) }
{ FN TIMESTAMPDIFF( SQL_TSI_MINUTE, TIMESTAMP '2006-08-02 00:00:00', TIMESTAMP '2006-08-02 00:15:00' ) }