Mimic.Close

The Mimic.Close function allows a script to close the Mimic display on which the script is running.

Syntax

Mimic.Close()

Description

Closes the Mimic display on which the script is running.

Arguments

None

Returns

None

Example:

Mimic.Close


Disclaimer

ClearSCADA 2017 R3