Using a Script’s Context Sensitive Menu

When you are editing your script, you can use the script context sensitive menu to access some useful features. To display the context sensitive menu, position the cursor on the background of the Script Editor display and then click the right-hand mouse button.

The context sensitive menu contains these useful options:

Further Information

A different set of menu options are available when a script's context-sensitive menu is accessed in Debug Mode.


Disclaimer

ClearSCADA 2017 R3