Built-In User Groups

ClearSCADA has a single built-in User Group named 'Everyone'. Every user account that is created is automatically associated with the 'Everyone' User Group. On new installations the Everyone User Group is inactive and is not assigned any security permissions.

If you activate the 'Everyone' User Group (by adding it to the Security window) you should configure it with the minimum of permissions. For example, if the Read, Browse and View Alarms permissions are allocated to the ‘Everyone’ User Group, these permissions are made available to every user account on the system.

 

If you access the Security window for a point and set the Everyone User Group to have the Tune Limits permission, it means that every user will be able to tune the limits of the point.

To allow your system users greater access to items and features, you should create ‘configured’ User Groups and user accounts. You can then apply the required permissions to groups of users or individual user accounts as required.

NOTICE

SECURITY THREAT

As all configured User accounts are automatically a member of the Everyone User Group, the incorrect use of the User Group can compromise the security of the system. You should only allocate the minimum of permissions if this User Group is added to the Security Windows.
Failure to follow these instructions can result in equipment damage.



Disclaimer

ClearSCADA 2017 R3