Control

The Control actions perform a specific control on a database item. The control varies according to the type of database item and the plant with which it is associated.

The Control permission defines whether the user account or User Group has access to the Control actions. There are many different control actions, including Control, Initialize, Set Forecast, Remove Forecast, Send Message, Generate Report, Print Report, and Export Report.

Availability: Can be restricted via the Permission Restrictions settings (see Define whether any Permissions are Restricted).


Disclaimer

ClearSCADA 2017 R3