Considerations for Running ClearSCADA on Citrix and Remote Desktop Services

(Microsoft Remote Desktop Services was formerly known as Microsoft Terminal Services.)

There are several advantages to running ViewX or WebX on a Citrix server or Remote Desktop Services server:

However, while using ClearSCADA with Citrix or Remote Desktop Services has several benefits, there is also a cost - higher bandwidth is required. This is because the Citrix or Remote Desktop Services server(s) has to send graphics to each of its clients. High bandwidth is needed to allow quantities of graphics to be sent effectively.

So, if you are interested in running ClearSCADA on Citrix or Remote Desktop Services servers, you need to consider:

A Citrix/Remote Desktop Services agent will be able to advise you on a suitable setup for your requirements and the associated costs.


Disclaimer

ClearSCADA 2017 R3