Historic and Archive Data

ClearSCADA provides the facilities to retain historical data online and to archive historical data. ClearSCADA can generate the following types of historic data:

Historic data is generally retained online for a specified duration, after this period of time expires the data is deleted to allow space for new data. Modified historical data is retained online permanently when historic data enabled. To retain historic data permanently it can be Archiving.

Archives are used to:


Disclaimer

ClearSCADA 2017 R3