Server License Settings

Each ClearSCADA system requires a server license that defines which drivers are available, the number of database points permitted, the number of client commendations permitted etc.

Depending on the configuration of your system, each ViewX client may also need a license. For more information, see Associate a ViewX Client - System Connection with a Client License.

If you are using virtualization, you must acquire a separate license for each copy of ClearSCADA that runs on a virtual server (see Virtualization and Cloud).

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3