Set the Type of Server

The Server Configuration Tool’s System Configuration>Partners settings include Type, which you can use to define the type of server architecture to which the server you are configuring belongs. For example, if you are configuring a server that is to be a Standby server in a Triple Standby architecture, you should set the Type to Triple Standby.

The Type setting defines the server’s role in the system architecture and can be set to:


Disclaimer

ClearSCADA 2017 R3