Start and Stop the System Server

This section explains how to use the Service Manager. When you install ClearSCADA on a server, you need to setup the ClearSCADA server to run as a service so that you can start and stop the server when required. You may need to start, stop, and restart the ClearSCADA server when you make changes to certain parts of the server configuration.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3