Working with the ClearSCADA Server Configuration Tool

When you have started ClearSCADA as a service, you may need to make some alterations to the ClearSCADA server configuration. For example, you may need to change the Partners settings so that the ClearSCADA server is used as part of a multi-server system rather than the default Lone Server arrangement.

To make alterations to the ClearSCADA server configuration, you need to use the various features of the ClearSCADA Server Configuration Tool.

Before you begin to configure the server(s), you should familiarize yourself with the ClearSCADA Server Configuration Tool. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R3